This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP432E411Y-BGAEVM: MSP432E411Y-BGAEVM can't connect with XDS110 Debug Probe.

Part Number: MSP432E411Y-BGAEVM


Tool/software: Code Composer Studio

Yesterday I got MSP432E411Y-BGAEVM with XDS110 Debug Probe, new one.

And I followed the step by step to connect each other.

1. External power supply, +5V,GND ,

2. Jumper connect J8 .

3. Using JB  with 20pin - 10 pin adapter .

RJ45 Ethernet Led is normal brinking.

And setup ccs like this.

But I got error message.

Could you help me? 

And I press Test Connection .

[Start: Texas Instruments XDS110 USB Debug Probe_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\STELLA\AppData\Local\TEXASI~1\CCS\
ti\3\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Nov 21 2018'.
The library build time was '00:08:45'.
The library package version is '8.0.903.2'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '5' (0x00000005).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.

-----[Print the reset-command hardware log-file]-----------------------------

The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the XDS110 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for XDS110 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.

The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.

[End: Texas Instruments XDS110 USB Debug Probe_0]

  • Have you tried without the 5V and removing J8 to see if the debug probe is supplying 3V?

    -edit: I have been able to acquire a probe and test.  The 10-pin connector is not keyed.  Rotate 180 degrees so that the red part of the ribbon cable is closer to the 20-pin connector.

    Chris

**Attention** This is a public forum