Part Number: MSP430FR5994
Hello everybody
I am trying to initialize the RTC_C on the MSP430FR5994 Launchpad by assigning values from the time library.
when I use hard coded values in 0x00 format, the downstream coding behaves differently than when I use the variable assignment
as shown below. I thought the problem was a type mismatch and tried casting, examining values etc but I am unable to resolve the
problem- calendar is not interpreting the variable assignment the same way as the hard coded values. My RTC initialization uses
binary so this is not a hexadecimal issue. The time lbirary fields (tm_sec, tm_min, etc) are integers while calendar fields are uint8_t.
any help is greatly appreciated.
thanks
jim
void Init_RTC()
{
struct tm *info;
time_t rawtime; //type is long. used to hold encoded calendar time
time(&rawtime); //function to get current system time relative to 1/1/1970 measured in seconds
info=localtime(&rawtime); //returns pointer to tm structure that stores date and time
mktime(info); //normalize values
// really lame assignments for debug
uint8_t sec =(uint8_t)(info->tm_sec);
uint8_t min= (uint8_t)(info->tm_min);
uint8_t hours = (uint8_t)(info->tm_hour);
uint8_t weekDay = (uint8_t)(info->tm_wday);
uint8_t month = (uint8_t)(info->tm_mon);
uint8_t dayOfmonth = (uint8_t)(info->tm_mday);
uint8_t year = (uint8_t)(info->tm_year);
//Setup Current Time for Calendar
calendar.Seconds = sec; //0x25;
calendar.Minutes = min; //0x05;
calendar.Hours = hours; //0x0C; //12
calendar.DayOfWeek = weekDay;//0x00;
calendar.DayOfMonth = month;//0x05;
calendar.Month = month+1;//0x02;
calendar.Year = 0x07e3; //0x2019;
// Initialize RTC with the specified Calendar above
RTC_C_initCalendar(RTC_C_BASE,
&calendar,
RTC_C_FORMAT_BINARY); //using RTC_C_FORMAT_BCD scrambles file time stamp
RTC_C_setCalendarEvent(RTC_C_BASE,
RTC_C_CALENDAREVENT_MINUTECHANGE
);
RTC_C_clearInterrupt(RTC_C_BASE,
RTC_C_TIME_EVENT_INTERRUPT
);
RTC_C_enableInterrupt(RTC_C_BASE,
RTC_C_TIME_EVENT_INTERRUPT
);
//Start RTC Clock
RTC_C_startClock(RTC_C_BASE);
}