This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6047: demo application for MSP430FR6043 kit

Part Number: MSP430FR6047
Other Parts Discussed in Thread: MSP430FR6043, , EVM430-FR6043

Greetings.

I'm evaluating FR6043 kit, out-of-box firmware and USS demo application with default configuration. I have a couple of questions:

0. Where do I find the schematics for the kit?

1. How do I configure the kit for 1MHz ultrasonic transducers? Maximum allowed frequency in USS design center app is 550kHz, although the documentation states that transducers up to 2.5MHz can be used.

2. I tried building USS Gas Demo firmware with USS_F1_FREQ set to 1000000. This does seem to produce 1MHz pulse, but I don't see any signal on the second transducer

**Attention** This is a public forum