This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2619S-HT: How to program MSP430F2619S-HT

Part Number: MSP430F2619S-HT
Other Parts Discussed in Thread: MSP-FET

Hi,
Can I use www.ti.com/.../msp-ts430pm64 and http://www.ti.com/tool/msp-fet to flash/program MSP430F2619S-HT? If not what options do I have?
Regards,
Bezak
  • If you are using the PM64 package, then you can use the msp-ts430pm64.
    If you are using KGD die, then only option is to program in final hardware using an msp-fet or other compatible programmer.

    If this answers your question, please click "Verify it as the answer"
    Regards,
    Wade

**Attention** This is a public forum