Other Parts Discussed in Thread: MSP430F2013, MSP430FR2355
Tool/software: WEBENCH® Design Tools
Hello All,
I have study the reference datasheet of controller MSP430F4X single chip weigh scale. also sharing a link of datasheet.

I have seen & understand the below things as given in the datasheet.
Load cell capacity = 10kg
Excitation Voltage = 3V
Output = 2mv X 3V
= 6mV At full load(10kg)
output voltage at 10kg is 6mV & at 1g is 0.6uV
in order to resolve 1g, the LSB voltage of the used ADC should be 4 times smaller that, which is 0.6uV/4=0.15uV.
---------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
In our case we are using MSP430I2020 24bit(ADC) controller.
load cell capacity = 300kg
Here we also share datasheet of load cell for more clarification.0676.PFS-410.pdf
Excitation Voltage = 10V
Output = 2mv X 10V
= 20mV At full load(300kg)
output voltage at 300kg is 20mV & at 1g is 0.066uV
in order to resolve 1g, the LSB voltage of the used ADC should be 4 times smaller that, which is 0.066uV/4=0.0166uV.
Question:
1) Why we need to divide LSB voltage four times?
2) Which PGA gain setting will be suitable for reading with 300kg load cell?
3) Which is better, internal or external reference voltage?
4) What is the minimum voltage that can be sense by ADC pin of controller?