Part Number: MSP430G2413
Hi
Do we have MSP430 automotive level device list?
My customer want to use one similar to NXP S9KEAZN8AMTGR. Thanks.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430G2413
Hi
Do we have MSP430 automotive level device list?
My customer want to use one similar to NXP S9KEAZN8AMTGR. Thanks.

Hi Daniel,
Please view the legacy MSP430 selections below that are automotive qualified (as denoted by Q1):
| Generic Part Number | Q1 Datasheet | Frequency (MHz) | Flash (KB) | SRAM (KB) | GPIO | Timers (16-bit) | Brown Out Reset | USCI_A (UART/LIN/Irda/SPI) | USCI_B (I2C/SPI) | Comparators | Temp Sensor | ADC Type | ADC Channels | Watchdog | BSL | Temp | Package |
| MSP430G2001-Q1 | SLAS775 | 16 | 0.5 | 0.125 | 10 | 1 | Yes | Yes | -40 to 85 | 14TSSOP | |||||||
| 16QFN | |||||||||||||||||
| MSP430G2201-Q1 | SLAS775 | 16 | 2 | 0.125 | 10 | 1 | Yes | Yes | -40 to 85 | 14TSSOP | |||||||
| 16QFN | |||||||||||||||||
| MSP430G2211-Q1 | SLAS775 | 16 | 2 | 0.125 | 10 | 1 | Yes | Yes | Slope | Yes | -40 to 85 | 14TSSOP | |||||
| 16QFN | |||||||||||||||||
| MSP430G2231-Q1 | SLAS787 | 16 | 2 | 0.125 | 10 | 1 | Yes | 1 | Yes | 10-bit SAR | 8 | Yes | -40 to 85 | 14TSSOP | |||
| 16QFN | |||||||||||||||||
| MSP430G2333-Q1 | SLAS802 | 16 | 4 | 0.25 | 16 | 2 | Yes | 1 | 1 | Yes | 10-bit SAR | 8 | Yes | UART | -40 to 85 | 20TSSOP | |
| 24 | 28TSSOP | ||||||||||||||||
| MSP430G2453-Q1 | SLAS966 | 16 | 8 | 0.5 | 16 | 2 | Yes | 1 | 1 | Yes | Yes | 10-bit SAR | 8 | Yes | UART | -40 to 85 | 20TSSOP |
| 24 | 28TSSOP | ||||||||||||||||
| MSP430G2553-Q1 | SLAS966 | 16 | 16 | 0.5 | 16 | 2 | Yes | 1 | 1 | Yes | Yes | 10-bit SAR | 8 | Yes | UART | -40 to 85 | 20TSSOP |
| 24 | 28TSSOP | ||||||||||||||||
| MSP430F2252-Q1 | SLAS770 | 16 | 16 | 0.5 | 32 | 2 | Yes | 1 | 1 | 10-bit SAR | 12 | Yes | UART | -40 to 105 | 40VQFN | ||
| MSP430F2272-Q1 | SLAS770 | 16 | 32 | 1 | 32 | 2 | Yes | 1 | 1 | 10-bit SAR | 12 | Yes | UART | -40 to 105 | 40VQFN |
**Attention** This is a public forum