This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I am using the GNU v7.3.2.154 Compiler.
Using the code below, and watching the stack pointer: Every loop iteration the stack grows by 2 bytes.
What am I missing here?
#include <msp430.h>
#include "stacktest.h"
/**
* main.c
*/
int main(void)
{
int i= 0;
ar j;
WDTCTL = WDTPW | WDTHOLD; // stop watchdog timer
for (i=16;i>0;--i){
test_sub(j);
}
return 0;
}
#include "msp430fr5994.h"
typedef unsigned int ar[16];
extern void test_sub(ar);
#include "msp430fr5994.h"
.global test_sub
test_sub:
pushm.w #8,R11
popm.w #8,R11
ret
**Attention** This is a public forum