Part Number: MSP430F2132
Other Parts Discussed in Thread: MSP430FR2153
Thank You Sir
Please clear my doubt:
1) As per suggestion for my project i have finalized Temperature sensor LM74 and Microcontroller MSP430F2132. My need is to interface microcontroller with temperature sensor LM74 with spi interface and MONZA x-2k dura rfid chip with microcontroller through I2C. But,
in data sheet of MSP430F2132 pin number 9 10 11 12 13 are UCB and UCA pins,
But,
10 and 11 are SDA and SCA pins used for IIC interface and 13 14 are spi pins SIMO and SOMI but then which pin will be used for GSM and wifi since 13 and 14 pins are only for TX and RX used for UART
Please suggest me the pin connection for Temerature sensor(spi) rfid chip(iic) and gsm/wifi(uart).
one more thing what is difference between MSP430F2132 and MSP430F2132 EP
Please clear my doubt sir