This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430G2553: BREAKPOINT -> PWM STOPP

Part Number: MSP430G2553
Other Parts Discussed in Thread: TMS320F28069

Tool/software: Code Composer Studio

Hello,

Launchpad MSP-EXP430G2 -> MSP430G2553.

PWM on P2.2 and P1.6.

When the program runs on a BREAKPIONT, the PWM stops.

Can one adjust that somewhere, that the PWM keeps running, as with the
Picolo (TMS320F28069 ... ) series?

Or at least that the PWM outputs when reaching a BREAKPOINT
to assume a predeterminable state?

Hello,
found it -> DEBUGGOPTIONEN.
Unfortunately, there is a line below me

"No module clock control available on this device".

Is already a serious limitation.

Which MSP430 is it working on?
Is there somewhere a MSP430 table that says where and with which DEBUGGER it works?

Regards, Friedrich

**Attention** This is a public forum