Part Number: MSP432E401Y
Tool/software: TI-RTOS
Hi,,
I am using "nvsinternal" example program for my application.
Using that application i am able to write the data on to the flash memory and read the flash memory.
However i would like to write the data on to the specific memory location and read when needed.
As per the example the Base address is : 0xE0000 and sector size is: 0x4000. that means i can write the data from (0xE0000 to 0xE3FFF).
If at all i want to write the data to the location (0xE2000) then how to initialize the write address to the nvs handle while writing and reading the location.
Thank you
Regards
Kalyan.