This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSS721A: TSS721A

Part Number: TSS721A


Hello, 

About the usage of TSS721A, the datasheet Page4 described like this:

"Beacause  the TSS721A is configured for half-duplex only, the current modulation from RX or RXI is repeated concurrently as ECHO on the outputs TX and TXI. If the slave, as well as the master, is trying to send information via the lines, the added signals appear on the outputs TX and TXI, which indicates the data collision to the slave"

So I'd like to confirm how to prevent the data collision? In other words, I don't hope the signals from RXI to appear on the output TX, how to do?   

Best regards

Kailyn 

**Attention** This is a public forum