Part Number: MSP430G2231
I am doing some tests using the MSP430G2231 ADC10 and I am seeing unexpected results when using external VREF- . I am not sure if I have set something up incorrectly or I am misunderstanding how it should work.
In the test circuit I can alter the offset between VREF- and MSP430G2231 supply GND. The input signal that I am reading is also offset with VREF- so that when measuring between the ADC input channel and VREF- the voltage reading is always constant regardless of the offset. I was expecting that the ADC reading would remain constant (within error margins) but what I am seeing is the ADC reading increases as the offset to GND is increased.
Any insight of advice would be appreciated.
This is how I have the ADC10 configured.
WDTCTL = WDTPW + WDTHOLD; BCSCTL1 = CALBC1_1MHZ; DCOCTL = CALDCO_1MHZ; ADC10AE0 |= BIT3 + BIT7; ADC10CTL0 = SREF_5 + ADC10SHT_3 + REFON + ADC10ON; ADC10CTL1 = INCH_7 + ADC10SSEL_2; __delay_cycles(1000); ADC10CTL0 |= ENC + ADC10SC; while (ADC10CTL1 & ADC10BUSY);
Alastair