Part Number: MSP430FR2532
Tool/software: Code Composer Studio
hi i am implementing 2 capacitive key using msp430fr2532 , i want to make a application in which when i touch a key the corresponding led should turn on . i have used CAP0.2 and CAP0.3 for switches .my LEDs are connected to P1.0 and P1.1 .
problem:-
1 ) initall when the code was generated no any led was glowing when i touched the key but then i changed the bits of LED1 and LED2
by assigning P1.0 as BIT0 and P1.1 as BIT1
#define LED1_PIN (BIT0)
#define LED2_PIN (BIT1)
but my led 2 is not working (is it right to assign BIT1 to P1.1 of msp430fr2532).
2) when i press any key only LED connected to P1.0 turns on while i want to turn it on only when key one is pressed .