This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/UNIFLASH: How prevent "Run Target After Program Load/Flash Operation" from command line interface?

Part Number: UNIFLASH
Other Parts Discussed in Thread: MSP430G2955

Tool/software: Code Composer Studio

I'm using UniFlash 4.6.0 to load software to an MSP430G2955. I need to not "Run Target After Program Load/Flash Operation". On the GUI, I can manually de-select the checkbox, but this option isn't included with the session settings when generating a standalone command line package.

What option should I specify when running dslite.bat from the command line to prevent the software from running immediately after it's flashed?

**Attention** This is a public forum