This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP432E411Y: ROV does not interprete %f

Part Number: MSP432E411Y

Tool/software: Code Composer Studio

Dear TI-Experts,

I'm using the following code for logging float data:

                    Log_print2(Diags_USER4, "ADC_Sensitive: Offset to high: %d lsb = %f uV",
                               self->ADC_PeriodicHandlerOffset, floatToArg(ofs*1.0e6));

ofs is a float variable. Logger is LoggerStopMode.

When using RTOS Analyzer -> Printf and Error Logs I see the right value for ofs displayed after stopping the µC.

But in ROV -> LoggerStopMode I only see "f", but no value. When using integers and %d everything is fine.

I assume, that %f is currently not implemented in ROV? Could you add this feature? Thank you in advance!

**Attention** This is a public forum