Part Number: EVM430-FR6047
Tool/software: Code Composer Studio
Hi,
I measured the current consumption of the evaluation module with transducer attached(no external peripherals) running the default code (LPM-active) .
When i removed the jumper J32 and measured current across the pin i got around 7µA.
But when i measured line current i was getting around 91mA.
1) Isn't total power consumption linked to line current?
2) Is the LPM ratings given in datasheet only for MCU excluding peripheral modules?
Regards,
Divya Harikumar