Part Number: MSP430F249
Other Parts Discussed in Thread: MSP430F2419
Hello.........
Can I expand the programmable flash memory size of msp430f249 from 60kb to some extent.( say 80kb or more ).
Is it possible to do so ?
If yes , HOW ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F249
Other Parts Discussed in Thread: MSP430F2419
Hello.........
Can I expand the programmable flash memory size of msp430f249 from 60kb to some extent.( say 80kb or more ).
Is it possible to do so ?
If yes , HOW ?
Hello Tharuvani,
probably the best fit, being the closest to the MSP430F249 is the MSP430F2419. It is available in the same package, offers the same feature set, but 120kB FLASH and 4KB RAM. As far as I can see fully pin compatible. One thing you need to keep in mind, due to the 120kB code memory, it has a 20Bit CPU, to avoid paging (linear address range maintained). This means it offers a few additional instructions, but the instruction set is a super set of the 16Bit MSP430 devices. Thus the code differences, if any will be minor, especially when you're writing code in C and not in assembler, basically most of the things will be fully transparent for you.
For further details, please see the device datasheet and the User's Guide.
Best regards
Peter
how can i get samples of msp430f2419 from TI.
it is showing limit the cart to 0 items, even i request samples from company mail address.
How can i get samples now from TI ?
what is the solution for cart limit to 0 ?
**Attention** This is a public forum