Part Number: MSP430FR5969
Other Parts Discussed in Thread: MSP-FET, ,
Executive Summary: I'm looking for a recommendation for a USB-UART adapter with additional GPIO to connect to the TST and ! RST pins.
Long version:
I am developing products based on the MSP430FR5969, and I use the UART to send commands back and forth with the larger system under normal operation (not SW update). I'm interested in using the built-in bootloader via eUSCI_A0 to allow software updates as well, and I'd like to use the TST/!RST pins to enter the BSL. If I were doing this on the MSP430FR59691, which has the I2C BSL, I could use my Aardvark, which includes additional GPIO on top of the I2C. I have an MSP-FET for programming and debugging, but it seems like it only supports full JTAG, not generic UART operation with added GPIO features.
Does anyone have a suggested UART-USB interface that I can use for testing with my development system? I have had the TUMPA recommended, but it seems like UART and JTAG interfaces can't be combined in this way. (Although I haven't purchased one to try it yet.)
Thanks,
Paul