Part Number: MSP430G2553
Other Parts Discussed in Thread: DRV8313, TIDA-00274
Customer is trying to use DRV8313 eval system to test a low inductance BLDC. Motor can run up to 25k rpm. When running from DRV8313 eval board with its GUI, the motor has high pk-pk current ripple due to the low L/R constant (L = 0.1mH, R = 1.8 ohm).
This could be addressed by operating the driver at a higher PWM frequency, closer to 200 kHz.
Can the insta-spin code that is part of the TIDA-00274 be modified to operate at such a PWM rate? If so, can you help point to where in the code to make the timer modifications?