This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Ive been trying to interface a 2 inch display driven by an ST7789 driver to MSP430FR6989.
The library is for arduino for the display adafruit with the same driver IC i added the library and tested the graphics test.ino where the compiler area was filled with errors which i have no idea so can anybody please help me with this i attached the libraries and the screenshots. I used the graphictest.ino from the Arduino-ST7789-Library-spi9bit and the gfx.h and cpp are there in the adafruit gxf library which i added both to the library section. and here is the link for lcd i used https://www.mouser.in/datasheet/2/271/Microtips%20Technology-8-1-2017-MTD0200FZS%20SPEC1-1181287.pdf
Adafruit-GFX-Library-master.zipArduino-ST7789-Library-spi9bit.zip
**Attention** This is a public forum