Part Number: MSP430F5659
Successfully computed CRC value using Block Transfer DMA mode, but when changing to using Burst-Block DMA mode then an incorrect value is computed. Only difference in code is a change in the DMADT value from 5 to 6 (or 7) in the DAM4CTL register. Using DMA channel 4. Does the DMA buffer size have to be a multiple of 4?