Hi
I am trying to setup an MPSP432P401R as an I2C multimaster. Is there an example code available to do/ understand the same? I used the code composer studio I2C example code to have the MSP432 MCU currently working as an ordinary master with the necessary read/write operations being performed with the multiple connected slaves on the bus. I now need to modify the current working code to multimaster mode as the necessity has arise to have two master MCUs on the same I2C bus.
I am fairly new to I2C programming and by reading the MSP432 technical manual and previous forum posts, I couldn't understand what needs to be done. Is there a flowchart somewhere to help me understand the MSP432 multimaster operation? In the MSP432 peripheral user guide (pg. 169), I found two functions mentioned for enabling and disabling multimaster mode in driverlib but I am unsure how to use them in my code.
Any help or guidance would be highly appreciated.
Thank You.