Part Number: MSP430F2370
Other Parts Discussed in Thread: TRF7970A, , TRF7960A
Hi,
I'm planning for a custom NFC reader board using MSP430F2370 and TRF7970A. I have a few questions
1. Is example code available for MSP430F2370 to develop NFC reader with TRF7970A ? If so where can I find it ?
2. I also have a LIN transceiver(TJA1020) in my custom board and will be using same MSP430F2370 to develop Lin slave application. Does MSP430F2370 support connection to both TRF7970A and Lin transceiver(TJA1020) ? For TRF7970A a SPI port is needed and for LIN transceiver UART is needed.
3. Does MSP430F2370 has an example code for LIN protocol ? If so where can I find it ?
4. Does MSP430F2370 has enough memory to handle NFC reader and LIN protocol app ? If not which micro do you recommend ?