Hi,
We where using the Rev A of the MSP430F5659 and everything worked fine, we lately moved to the Rev B. and the boards are not working correctly means that the SW is stuck, is there any reason for that? any differences between the Rev A and B?
We are using external 19.2MHz clock, the SW is working fine with the internal clock but when moving to the external (XT2) the SW is stuck,
Many Thanks,
HRi