Part Number: MSP430F6659
Other Parts Discussed in Thread: MSP430F6638,
Tool/software: TI C/C++ Compiler
Hi Team,
One of our customer facing an issue in existing code compilation with new device MS430F6659 with IAR v7.10.3.
Customer Details :
Details:
Customer have an existing system with software code, which they are able to compile with MSP430F6638 device flag.
When they selected the MSP430F6659 option from IAR project options, Compilation failed because this CPU flag check is not present in USB/USB_API/USB_Common/device.h file which they guess is provided by TI.
Snapshot is attached below for your reference.
Could you advice, is it safe for customer to add check for __MSP430F6659__ in existing file ?
If possible, can you provide IAR v4.42a as well.
Thanks and regards,
Don