Part Number: MSP430G2553
Tool/software: TI C/C++ Compiler
Hi,
We have implemented the example code to check the storage onto the MSP430 information memory.
The below is the code for it
#include <msp430g2553.h>
void WriteCharToFlash(char* Flashptr, char val);
void WriteLongToFlash(long* Flashptr, long val);
void ReadCharFromFlash(char* address, char* val);
void ReadLongFromFlash(long* address, long* val);
void ClearAllFlash();
void EraseSegment(char *flash_ptr);
int main(void) {
WDTCTL = WDTPW + WDTHOLD;
BCSCTL1 = CALBC1_1MHZ; // Set DCO to 1MHz
DCOCTL = CALDCO_1MHZ;
FCTL2 = FWKEY + FSSEL_3 + FN1;
char val;
char val2;
char val3;
//ClearAllFlash();
EraseSegment((char*) 0x1000);
WriteCharToFlash((char *) 0x01000, '1');
WriteCharToFlash((char *) 0x01004, '3');
WriteCharToFlash((char *) 0x01008, '5');
ReadCharFromFlash((char *) 0x01000, &val2);
ReadCharFromFlash((char *) 0x01004, &val);
ReadCharFromFlash((char *) 0x01008, &val3);
return 0;
}
void WriteLongToFlash(long* address, long val)
{
long* flash_ptr;
flash_ptr = address; // Initialize Flash pointer
while(FCTL3 & BUSY);
FCTL1 = FWKEY + WRT;
*flash_ptr = val;
while(FCTL3 & BUSY);
FCTL1 = FWKEY; // Clear WRT bit
FCTL3 = FWKEY + LOCK; // Set LOCK bit
}
void ReadLongFromFlash(long* address, long* val)
{
while(FCTL3 & BUSY);
long* flash_ptr;
flash_ptr = address;
*val = *flash_ptr;
}
void WriteCharToFlash(char* address, char val)
{
char* flash_ptr;
flash_ptr = address; // Initialize Flash pointer
while(FCTL3 & BUSY);
FCTL1 = FWKEY + WRT;
*flash_ptr = val;
while(FCTL3 & BUSY);
FCTL1 = FWKEY; // Clear WRT bit
FCTL3 = FWKEY + LOCK; // Set LOCK bit
}
void ReadCharFromFlash(char* address, char* val)
{
while(FCTL3 & BUSY);
char* flash_ptr;
flash_ptr = address;
*val = *flash_ptr;
}
/*void ClearAllFlash()
{
char *flash_ptr; // Segment D pointer
flash_ptr = (char *) 0x1000; // Initialize Flash segment D pointer
FCTL1 = FWKEY + MERAS; // Set Mass Erase bit
FCTL3 = FWKEY; // Clear Lock bit
*flash_ptr = 0; // Dummy write to erase Flash segment D
FCTL1 = FWKEY + WRT; // Set WRT bit for write operation
FCTL1 = FWKEY; // Clear WRT bit
FCTL3 = FWKEY + LOCK;
}*/
void EraseSegment(char *flash_ptr)
{
FCTL3 = FWKEY; // Clear Lock bit
FCTL1 = FWKEY + ERASE; // Set Erase bit
*flash_ptr = 0;
FCTL1 = FWKEY; // Clear WRT bit
FCTL3 = FWKEY + LOCK; // Set LOCK bit
}
While debugging the above code i am not able to see any change on the Information memory.Find the below picture.