Part Number: MSP432E411Y
Other Parts Discussed in Thread: MSP-EXP432E401Y
Dear TI-Expert,
I'm trying to get software updates for our product working. Could you provide some example code how to use ROM_UpdateUART and ROM_UpdateUSB?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432E411Y
Other Parts Discussed in Thread: MSP-EXP432E401Y
Dear TI-Expert,
I'm trying to get software updates for our product working. Could you provide some example code how to use ROM_UpdateUART and ROM_UpdateUSB?
Hello Sven,
We don't have specific code examples that show how to use ROM_UpdateUART and ROM_UpdateUSB APIs, but I can provide a brief summary of what to do before these APIs are called:
For USB:
For UART - The function SoftwareUpdateBegin in the file "./source/third_party/lwip/ports/msp432e4/utils/swupdate.c" demos the following steps for Ethernet.
Hope this helps!
Thanks,
Sai
Hello Sai,
thank you for your answer. I already had a look into the bootloader examples and derived (almost copied) the following code:
#define TIMESTAMP_CLOCK 120000000ULL
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
/* Set GPIO PA0 and PA1 as UART. */
MAP_GPIOPinConfigure(GPIO_PA0_U0RX);
MAP_GPIOPinConfigure(GPIO_PA1_U0TX);
MAP_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
/* Configure the UART for 115200, n, 8, 1 */
MAP_UARTConfigSetExpClk(UART0_BASE, TIMESTAMP_CLOCK, 115200,
(UART_CONFIG_PAR_NONE | UART_CONFIG_STOP_ONE |
UART_CONFIG_WLEN_8));
/* Enable the UART operation. */
MAP_UARTEnable(UART0_BASE);
/* We must make sure we turn off SysTick and its interrupt before entering
* the boot loader! */
MAP_SysTickIntDisable();
MAP_SysTickDisable();
/* Disable all processor interrupts. Instead of disabling them one at a
* time, a direct write to NVIC is done to disable all peripheral
* interrupts. */
NVIC->ICER[0] = 0xffffffff;
NVIC->ICER[1] = 0xffffffff;
NVIC->ICER[2] = 0xffffffff;
NVIC->ICER[3] = 0xffffffff;
ROM_UpdateUART();
According to SPMU363 (Tiva™ C Series TM4C129x ROM USER’S GUIDE) the UART peripheral must be configured and operational before calling ROM_UpdateUART. I checked the UART by sending a few symbols. It works at the expected bitrate of 115200bit/s.
Unfortunately this code is not working at all on our MSP432E411Y hardware (BSL scripter gets no response from BSL neither with nor without DISABLE_AUTO_BAUD option).
After a mass erase I get the blinky example programmed and running, thus connection seems OK.
Honestly I cannot imagine, that there is no code available at TI. Someone must have done testing on the ROM_UpdateUART function.
I already spent an unexpected amount of time on getting the MSP432E programmed via UART and it is still not working. The only thing I could get till now is programming our hardware with the blinky example after a mass erase via the MSP-EXP432E401Y's UART and BSL scripter. Programming our real software on the hardware the same way failed - BSL scripter reported everthing ok after 4 minutes, but the application ended in an endless loop. (The same application is running fine after programming via USB/LMFlasher or JTAG/CCS.)
I'm really frustrated.
Please ask the developer for a working code example!
Hello Sai,
the reason for our application not being programmed correctly by BSL scripter might be a function in RAM (__attribute__((ramfunc))) resulting in follwing entry in the .txt file:
@23cd0
Maybe BSL scripter is unable to deal with it.
Hello Sai,
now I used LM flasher for the serial programming, too. It simply works, thus the code above is fine. When using the explicit ROM_UpdateUART function it even works with a standard USB to RS232 converter.
Why is TI promoting BSL scripter instead of LM flasher??
Hello Sven,
Thanks for the updates! I will talk to the development team to investigate the issues that you reported.
Regards,
Sai
**Attention** This is a public forum