Other Parts Discussed in Thread: CC3220SF-LAUNCHXL
Hi there,
I've programmed an MSP-EXP430FR5739 launchpad with a simple application to send data by the serial UART. I connected the launchpad to a pc using the USB cable and I used the terminal included in CCS 9 to read this data using a serial virtual com.
When I plug the launchpad in a PC with Windows 10 HOME, it works. I can read the data sent by the microcontroller.
When I plug the launchpad in a PC with Windows 10 EDUCATION, it doesn't work, that is, nothing is received.
I tried with several PCs, launchpads and cables, and also with putty and Hercules terminal, and the behaviour is always the same: Windows 10 HOME works, Windows 10 EDUCATION doesn't work
Even I've checked with two PCs with Windows 10 EDUCATION, connecting them using two USB-Serial adapter and I can send and receive data to/from each PC using the terminal included in CCS 9.
Is there a problem with the MSP430 Application UART driver in Windows 10 EDUCATION?
Thanks for your help,
Toni.