Tool/software: Code Composer Studio
External temperature and humidity sensor with single bus communication,Send according to the required timing, but can not get the low-level response of the sensor, want to know where the configuration is wrong.
The following is the source code configuration and implementation of the original 51 MCU:
#include <reg51.h>
#include <intrins.h>
//
typedef unsigned char U8; /* defined for unsigned 8-bits integer variable 无符号8位整型变量 */
typedef signed char S8; /* defined for signed 8-bits integer variable 有符号8位整型变量 */
typedef unsigned int U16; /* defined for unsigned 16-bits integer variable 无符号16位整型变量 */
typedef signed int S16; /* defined for signed 16-bits integer variable 有符号16位整型变量 */
typedef unsigned long U32; /* defined for unsigned 32-bits integer variable 无符号32位整型变量 */
typedef signed long S32; /* defined for signed 32-bits integer variable 有符号32位整型变量 */
typedef float F32; /* single precision floating point variable (32bits) 单精度浮点数(32位长度) */
typedef double F64; /* double precision floating point variable (64bits) 双精度浮点数(64位长度) */
//
#define uchar unsigned char
#define uint unsigned int
#define Data_0_time 4
//----------------------------------------------//
//----------------IO口定义区--------------------//
//----------------------------------------------//
sbit P2_0 = P2^0 ;
//----------------------------------------------//
//----------------定义区--------------------//
//----------------------------------------------//
U8 U8FLAG,k;
U8 U8count,U8temp;
U8 U8T_data_H,U8T_data_L,U8RH_data_H,U8RH_data_L,U8checkdata;
U8 U8T_data_H_temp,U8T_data_L_temp,U8RH_data_H_temp,U8RH_data_L_temp,U8checkdata_temp;
U8 U8comdata;
U8 outdata[5]; //定义发送的字节数
U8 indata[5];
U8 count, count_r=0;
U8 str[5]={"RS232"};
U16 U16temp1,U16temp2;
SendData(U8 *a)
{
outdata[0] = a[0];
outdata[1] = a[1];
outdata[2] = a[2];
outdata[3] = a[3];
outdata[4] = a[4];
count = 1;
SBUF=outdata[0];
}
void Delay(U16 j)
{ U8 i;
for(;j>0;j--)
{
for(i=0;i<27;i++);
}
}
void Delay_10us(void)
{
U8 i;
i--;
i--;
i--;
i--;
i--;
i--;
}
void COM(void)
{
U8 i;
for(i=0;i<8;i++)
{
U8FLAG=2;
while((!P2_0)&&U8FLAG++);
Delay_10us();
Delay_10us();
Delay_10us();
U8temp=0;
if(P2_0)U8temp=1;
U8FLAG=2;
while((P2_0)&&U8FLAG++);
//超时则跳出for循环
if(U8FLAG==1)break;
//判断数据位是0还是1
// 如果高电平高过预定0高电平值则数据位为 1
U8comdata<<=1;
U8comdata|=U8temp; //0
}//rof
}
//--------------------------------
//-----湿度读取子程序 ------------
//--------------------------------
//----以下变量均为全局变量--------
//----温度高8位== U8T_data_H------
//----温度低8位== U8T_data_L------
//----湿度高8位== U8RH_data_H-----
//----湿度低8位== U8RH_data_L-----
//----校验 8位 == U8checkdata-----
//----调用相关子程序如下----------
//---- Delay();, Delay_10us();,COM();
//--------------------------------
void RH(void)
{
//主机拉低18ms
P2_0=0;
Delay(180);
P2_0=1;
//总线由上拉电阻拉高 主机延时20us
Delay_10us();
Delay_10us();
Delay_10us();
Delay_10us();
//主机设为输入 判断从机响应信号
P2_0=1;
//判断从机是否有低电平响应信号 如不响应则跳出,响应则向下运行
if(!P2_0) //T !
{
U8FLAG=2;
//判断从机是否发出 80us 的低电平响应信号是否结束
while((!P2_0)&&U8FLAG++);
U8FLAG=2;
//判断从机是否发出 80us 的高电平,如发出则进入数据接收状态
while((P2_0)&&U8FLAG++);
//数据接收状态
COM();
U8RH_data_H_temp=U8comdata;
COM();
U8RH_data_L_temp=U8comdata;
COM();
U8T_data_H_temp=U8comdata;
COM();
U8T_data_L_temp=U8comdata;
COM();
U8checkdata_temp=U8comdata;
P2_0=1;
//数据校验
U8temp=(U8T_data_H_temp+U8T_data_L_temp+U8RH_data_H_temp+U8RH_data_L_temp);
if(U8temp==U8checkdata_temp)
{
U8RH_data_H=U8RH_data_H_temp;
U8RH_data_L=U8RH_data_L_temp;
U8T_data_H=U8T_data_H_temp;
U8T_data_L=U8T_data_L_temp;
U8checkdata=U8checkdata_temp;
}//fi
}//fi
}
//----------------------------------------------
//main()功能描述: AT89C51 11.0592MHz 串口发
//送温湿度数据,波特率 9600
//----------------------------------------------
void main()
{
U8 i,j;
//uchar str[6]={"RS232"};
/* 系统初始化 */
TMOD = 0x20; //定时器T1使用工作方式2
TH1 = 253; // 设置初值
TL1 = 253;
TR1 = 1; // 开始计时
SCON = 0x50; //工作方式1,波特率9600bps,允许接收
ES = 1;
EA = 1; // 打开所以中断
TI = 0;
RI = 0;
SendData(str) ; //发送到串口
Delay(1); //延时100US(12M晶振)
while(1)
{
//------------------------
//调用温湿度读取子程序
RH();
//串口显示程序
//--------------------------
str[0]=U8RH_data_H;
str[1]=U8RH_data_L;
str[2]=U8T_data_H;
str[3]=U8T_data_L;
str[4]=U8checkdata;
SendData(str) ; //发送到串口
//读取模块数据周期不易小于 2S
Delay(20000);
}//elihw
}// main
void RSINTR() interrupt 4 using 2
{
U8 InPut3;
if(TI==1) //发送中断
{
TI=0;
if(count!=5) //发送完5位数据
{
SBUF= outdata[count];
count++;
}
}
if(RI==1) //接收中断
{
InPut3=SBUF;
indata[count_r]=InPut3;
count_r++;
RI=0;
if (count_r==5)//接收完4位数据
{
//数据接收完毕处理。
count_r=0;
str[0]=indata[0];
str[1]=indata[1];
str[2]=indata[2];
str[3]=indata[3];
str[4]=indata[4];
P0=0;
}
}
}
Here is the code I modified according to the above program:
#include "msp.h"
#include <stdint.h>
#include "../inc/LaunchPad.h"
#include "../inc/Clock.h"
#include "string.h"
#include "../inc/UART0.h"
/**
* main.c
*/
typedef unsigned char U8; /* defined for unsigned 8-bits integer variable 无符号8位整型变量 */
typedef signed char S8; /* defined for signed 8-bits integer variable 有符号8位整型变量 */
typedef unsigned int U16; /* defined for unsigned 16-bits integer variable 无符号16位整型变量 */
typedef signed int S16; /* defined for signed 16-bits integer variable 有符号16位整型变量 */
typedef unsigned long U32; /* defined for unsigned 32-bits integer variable 无符号32位整型变量 */
typedef signed long S32; /* defined for signed 32-bits integer variable 有符号32位整型变量 */
typedef float F32; /* single precision floating point variable (32bits) 单精度浮点数(32位长度) */
typedef double F64; /* double precision floating point variable (64bits) 双精度浮点数(64位长度) */
#define uchar unsigned char
#define uint unsigned int
#define Data_0_time 4
void DATA_init(void){
P5->SEL0 &= ~0x01;
P5->SEL1 &= ~0x01;
P5->DIR |= 0x01; // 2) make P1.4 and P1.1 out
P5->REN &= ~0x01; // 3) enable pull resistors on P1.4 and P1.1
P5->OUT |= 0x01; // P1.4 and P1.1 are pull-up
}
U8 U8FLAG,k;
U8 U8count,U8temp;
U8 U8T_data_H,U8T_data_L,U8RH_data_H,U8RH_data_L,U8checkdata;
U8 U8T_data_H_temp,U8T_data_L_temp,U8RH_data_H_temp,U8RH_data_L_temp,U8checkdata_temp;
U8 U8comdata;
U8 outdata[5]; //定义发送的字节数
U8 indata[5];
U8 count, count_r=0;
U8 str[5]={"RS232"};
U16 U16temp1,U16temp2;
void COM(void)
{
U8 i;
for(i=0;i<8;i++)
{
U8FLAG=2;
while((!(P5->IN&0x01))&&U8FLAG++);
Clock_Delay1us(30);
U8temp=0;
if(P5->IN&0x01)U8temp=1;
U8FLAG=2;
while((P5->IN&0x01)&&U8FLAG++);
//超时则跳出for循环
if(U8FLAG==1)break;
//判断数据位是0还是1
// 如果高电平高过预定0高电平值则数据位为 1
U8comdata<<=1;
U8comdata|=U8temp; //0
}//rof
}
void RH(void)
{
//主机拉低18ms
P5->DIR |= 0x01;
//P5->OUT |= 0x01;
P5->OUT &= ~0x01;
Clock_Delay1ms(18);
P5->OUT |=0x01;
//总线由上拉电阻拉高 主机延时20us
Clock_Delay1us(20);
//主机设为输入 判断从机响应信号
P5->DIR &= ~0x01;
//判断从机是否有低电平响应信号 如不响应则跳出,响应则向下运行
if(!(P5->IN&0x01)) //T ! //It is never possible to detect a low level signal here.
{
U8FLAG=2;
//判断从机是否发出 80us 的低电平响应信号是否结束
while((!(P5->IN&0x01))&&U8FLAG++);
U8FLAG=2;
//判断从机是否发出 80us 的高电平,如发出则进入数据接收状态
while((P5->IN&0x01)&&U8FLAG++);
//数据接收状态
COM();
U8RH_data_H_temp=U8comdata;
COM();
U8RH_data_L_temp=U8comdata;
COM();
U8T_data_H_temp=U8comdata;
COM();
U8T_data_L_temp=U8comdata;
COM();
U8checkdata_temp=U8comdata;
// P5->DIR |=0x01;
// P5->OUT |=0x01;
//数据校验
U8temp=(U8T_data_H_temp+U8T_data_L_temp+U8RH_data_H_temp+U8RH_data_L_temp);
if(U8temp==U8checkdata_temp)
{
U8RH_data_H=U8RH_data_H_temp;
U8RH_data_L=U8RH_data_L_temp;
U8T_data_H=U8T_data_H_temp;
U8T_data_L=U8T_data_L_temp;
U8checkdata=U8checkdata_temp;
}//fi
}//fi
}
//------------UART0_OutChar------------
// Output 8-bit to serial port
// Input: letter is an 8-bit ASCII character to be transferred
// Output: none
void UART_OutChar(U8 letter){
while((EUSCI_A0->IFG&0x02) == 0);
EUSCI_A0->TXBUF = letter;
}
//------------UART0_OutString------------
// Output String (NULL termination)
// Input: pointer to a NULL-terminated string to be transferred
// Output: none
void UART_OutString(U8 *pt){
while(*pt){
UART_OutChar(*pt);
pt++;
}
}
void main(void)
{
Clock_Init48MHz(); // 48 MHz clock; 12 MHz Timer A clock
UART0_Init();
DATA_init();
UART_OutString("11111111111111");
Clock_Delay1ms(100);
while(1)
{
//------------------------
//调用温湿度读取子程序
RH();
//串口显示程序
//--------------------------
str[0]=U8RH_data_H;
str[1]=U8RH_data_L;
str[2]=U8T_data_H;
str[3]=U8T_data_L;
str[4]=U8checkdata;
UART_OutString(str) ; //发送到串口
UART_OutChar('\n');
//读取模块数据周期不易小于 2S
Clock_Delay1ms(2000);
}//elihw
}
Is there any other example of single bus operation?