Part Number: EVM430-FR6043
Other Parts Discussed in Thread: MSP430FR6043
Hello,
This is the question with the follow up on the previous one.
I need to generate a pulse signal which has a width of the total number of pulses generated at the output of the Channel_0 out pin of the MSP430FR6043. the signal which needs to be generated is as shown below for better understanding. below you can see 4 pulses generated at the output (yellow) and (red) pulse signal which is desired to be generated on the XPBO pin which is free to use in the current evaluation board.
Then I tried to vary the RExN pin to fit the pulses but it is not possible. Then I decided to use the XPBO pin i.e Pin P7.0 which is not used in the current program. So with the help of Google, I wrote a small program to make the P7.0 pin high and then again make it low and also the main point here is to find the perfect loop to place this program so I can get the desired signal (red).
I tried a few loops and the results are as shown below.
I got the pulse signal which covers both the pulse upstream and downstream.
My question:
Where can I find the perfect loop to place my program where i can generate the desired pulse signal as shown above.
Thank you
BR
Jadhav