Hi,
I am currently starting the design of a board using MSP432E401Y and we want to use both Ethernet and USB.
As far as I understand the clock tree of the MSP432 I think it is not possible with the following constraints extracted from the datasheet:
- To use Ethernet, MSOSC shall be 25MHz
- For USB to work as expected, USBCLK shall be 60MHz
- PSYSDIV shall be 2
- SYSCLK shall be 240MHz or less
With (3) and (4) Fvco shall be 240MHz or less so.
With a Fvco lower than 240MHz there is no common multiple between 25 and 60MHz.
Can you confirm I am right?
Or did I made a mistake reading the datasheet and went in some kind of over constraints.
Best regards,
Frederic