Part Number: MSP430FR5870
Question: regarding the crypto bootloader from a code protection perspective, under the assumption I need this functionality.
I do no see where the MSP430FR5870 supports this feature. While our equipment is not networked and there is no way to connect to a remote system, we may perform firmware updates via boot strap loader from the main CPU board in the system indirectly from a USB stick. Would / does the crypto boot loader function between our CPU mother board and the MSP430 based attached board and secure the “in system” transfer of firmware?
Thanks
Viktorija