Part Number: MSP432E401Y
I have an application where I would like to generate 4 PWM signal that will all have the same time period but need independent control of the duty cycle and I want to use the fault input for fault protection. I also need one channel of input capture to measure a speed signal. It appears that you can only do one or the other with this processor. Is this correct? If not, how should it be configured?