Part Number: MSP430FR6047
Hello team,
Could you please advise the questions below:
- I need the ultrasonic measurement to yield the water flow speed (meter per second). How can I retrieve such result?
- I understand that its recommended to have at least 4 ultrasonic transducers when measuring water flow at pipe diameters 3’’ and above. Due to turbulence.
* Is that true?, If so, how does this TI chip handle such requirement? Do you have a procedure for that?
* Is there a recommended mounting position for the transducers on pipes with a diameter larger than 3’’? (I think the standard for 2 transducers is 3 and 9 o’clock – horizontally)
* According to your experience, mounting the transducers near pipe splitting or other pipe components will create more turbulence? If so, what is the recommended distance between the measurement location and pipe splitting/component?
3. Can you please explain the role of the config flag: “USS_ALG_HIGH_FLOW_OPTION“? Is that relevant to flow at pipes 3’’ or 4’’?
Thanks in advance
Kind regards,
Shai