Part Number: MSP430F5342
Dear TI experts,
Now I have some problems with lnk430f5342.xcl which is known as link file.The IDE which I'm using is IAR For MSP430.
1.What's the difference between LOW MEMORY 0-0FFFF and ALL MEMORY 0-FFFFF?
2.If I want to modify code range,can I set the code range like the picture as follow,LOW MEMORY:4400-FBFF and All MEMORY:4400-FBFF,10000-137FF,
and FC00-FFFF with nothing except interrupt vectors.
3.How can I set Interrupt Service Routine fixed?If I want to set ISR's address in the range 4400-FBFF,or 10000-137FF,what should I modify this .xcl?With the ISR in the range 10000-137FF,16bit interrupt vectors can pointer to the address over 0xFFFF?If not,which range should I choose?
4.In summary,if I want to set the code range in 4400-FBFF,10000-137FF,ISR in fixed address,is there any .xcl files to refer to about MSP430F5342?
Best Regards!