This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RE: CCS/CC430F5137: Can't connect to CC430F5137 with MSP-FET

Other Parts Discussed in Thread: MSP-FET

HI Chris

thank for interesting

i have done only half of work, becasue deugger seems to work correctly now, but i have issues with example code..

this example code use a LPRS RTOS, if i build and download .hex into device with LPRS serial bootloader everything works fine, if i debug or download program with MSP-FET something is missing and program goes in loop running ( and it's caused by missing commands, i can check that some instruction point to a blank memory area). i think that when i use MSP-FET it can't (obviusly) load the right LPRS RTOS, so i need to know how to do. note that the evaluation board of LPRS ( that i'm using) have a jtag connector biult in...

i need LPRS RTOS becasue it's alredy done for radio working and to use LPRS certified module.

i contacted also LPRS technical support but no one reply..

thank you very much

best regards

A.F.

**Attention** This is a public forum