Other Parts Discussed in Thread: MSP430G2553
As the title says I'm looking to develop an analog signal converter, or modifier to be more specific, using the 430G2553 chip.
To be more specific the project is to take the signal from an electric guitar/bass that has an on board pre-amp, pass it onto the board and modify the signal such as to imitate an effect pedal(distorted sound for example).
I know that I'll need to limit the voltage from the guitar's pre-amp from the 9V battery that it uses to 5V as to protect the board.
My question is if I will need anything else for the project like more amps for the signal after the modification and such. My knowledge of circuitry is limited for projects like that as I have recently started using microcontrollers and electronics, that is why I ask for any assistance that can be given. The type of signal that will be the finished product hasn't been decided yet for the reason that I might need to do some research on the conversion, but I'm pretty sure all modifications can be done through SW alone if I'm not mistaken to the capabilities of the chip. Also if this specific chip can't do the work I need you're welcome to point me to a TI one(or non if need be) that I can use to make my project.
Thanks in advance for any help given.
P.S Sorry if this isn't the right section of the forum to ask for such assistance, and this thread can be moved to the right section if needed.