Part Number: TIDM-1019
I recently purchased an eval board for the MSP430FR6047 Water Meter. I use transducers from Audiowell (same as those used in documention).
The pipe with transducers is on a testing bench with a flowrate (water) fixed at 500L/h.
I read the mean value of the flowrate on USS, and i'm able to calculate the new "Meter constant".
The problem is, when i want to change the default value (12742000.00) by the new one (33390985.00), i've the following error " Non-advanced parameter error : Invalid Meter Constant"
Can you help me ? I didn't find any solution in the documentation
i'm using this version : UltrasonicWaterFR604x_02_20_00_08
Best Regards,
Maxime