This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6043: Issue with SPI CLK (UCA2) when mapped to port PJ

Part Number: MSP430FR6043


I am having an issue with the SPI functionality on the MSP430FR6043 when trying to map it to port PJ (pins PJ.0-PJ.3). The MOSI signal on PJ.2 works fine, but the clock does not appear on PJ.0 at all. When mapped to port P5 (P5.0 - P5.3) everything works as expected. I double check the electrical connection by setting the PJ.0 as a digital IO and sending out some pulses, which registered on the scope correctly. I repeated this test on three separate devices, with the same results. I tried both with an SPI device connected, and with the MCU pin floating. I don't think the pins on port PJ are entering JTAG mode, the SYSJTAGPIN is 0, and the device behaves the same when debugging with SPW, as well as when running off battery with the SPW programmer disconnected and the RESET pin pulled high at all times. Could there be something else preventing the PJ.0 pin from muxing into the SPI clock on the UCA2 module? Please advice. I would really appreciate having these pins specifically available for that feature, as I am working with a very tight PCB layout, and the position of the USS module and the LCD is fixed, leaving me very little wiggle room.

Attached: scope trace from pin P5.2 (working) and PJ.0 (not working), and the test code I ran. The tests were performed on a custom PCB, with either the PJ.0 pin floating (connected only to a scope probe), or connected to an SPI slave device thought a 22R resistor. Debugged with an MSP FET, over a SBW connection with only the SBWCLK and SBWTDO pins connected. Thanks for any input!

#include "driverlib.h"

uint8_t RXData = 0;
uint8_t TXData = 0;
int i=0;

void main(void){
    //Stop watchdog timer
    WDT_A_hold(WDT_A_BASE);
    PMM_unlockLPM5();

    //Set DCO frequency to max DCO setting
    CS_setDCOFreq(CS_DCORSEL_0, CS_DCOFSEL_3);
    CS_initClockSignal(CS_SMCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1);

    //test CLK pins in output mode
    GPIO_setAsOutputPin(GPIO_PORT_PJ,BIT0);
    GPIO_setAsOutputPin(GPIO_PORT_P5,BIT2);

    //3 pulses
    for(i=0; i<6; i++){
        GPIO_toggleOutputOnPin(GPIO_PORT_PJ, BIT0);
        GPIO_toggleOutputOnPin(GPIO_PORT_P5, BIT2);
        __delay_cycles(1000);
    }


    //for PORT PJ (with CLK not working)
    GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_PJ, BIT0 | BIT1 | BIT2 | BIT3, GPIO_PRIMARY_MODULE_FUNCTION);

    //for PORT P5 (working fine)
    GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P5, BIT0 | BIT1 | BIT2 | BIT3, GPIO_SECONDARY_MODULE_FUNCTION);


    //Initialize Master
    EUSCI_A_SPI_initMasterParam param = {0};
    param.selectClockSource = EUSCI_A_SPI_CLOCKSOURCE_SMCLK;
    param.clockSourceFrequency = CS_getSMCLK();
    param.desiredSpiClock = 50000;
    param.msbFirst = EUSCI_A_SPI_MSB_FIRST;
    param.clockPhase = EUSCI_A_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT;
    param.clockPolarity = EUSCI_A_SPI_CLOCKPOLARITY_INACTIVITY_HIGH;
    param.spiMode = EUSCI_A_SPI_3PIN;
    EUSCI_A_SPI_initMaster(EUSCI_A2_BASE, &param);

    //Enable SPI module
    EUSCI_A_SPI_enable(EUSCI_A2_BASE);

    EUSCI_A_SPI_clearInterrupt(EUSCI_A2_BASE,EUSCI_A_SPI_RECEIVE_INTERRUPT);
    // Enable USCI_A0 RX interrupt
    EUSCI_A_SPI_enableInterrupt(EUSCI_A2_BASE,EUSCI_A_SPI_RECEIVE_INTERRUPT);

    //Wait for slave to initialize
    __delay_cycles(100);

    TXData = 0x1;                             // Holds TX data

    //USCI_A0 TX buffer ready?
    while (!EUSCI_A_SPI_getInterruptStatus(EUSCI_A2_BASE, EUSCI_A_SPI_TRANSMIT_INTERRUPT)) ;

    //Transmit Data to slave
    EUSCI_A_SPI_transmitData(EUSCI_A2_BASE, TXData);

    __bis_SR_register(LPM0_bits + GIE);      // CPU off, enable interrupts
    __no_operation();                       // Remain in LPM0
}

#pragma vector=USCI_A2_VECTOR
__interrupt
void USCI_A2_ISR(void){
    switch(__even_in_range(UCA2IV, USCI_SPI_UCTXIFG))
    {
        case USCI_SPI_UCRXIFG:      // UCRXIFG
            //USCI_A0 TX buffer ready?
            while (!EUSCI_A_SPI_getInterruptStatus(EUSCI_A2_BASE,EUSCI_A_SPI_TRANSMIT_INTERRUPT));

            RXData = EUSCI_A_SPI_receiveData(EUSCI_A2_BASE);

            //Increment data
            TXData++;

            //Send next value
            EUSCI_A_SPI_transmitData(EUSCI_A2_BASE,TXData);

            //Delay between transmissions for slave to process information
            __delay_cycles(40);
            break;
        default:
            break;
    }
}

  • Hi Marek,

    I am looking into this and will provide an update early next week.

    Thanks,

    Mitch

  • Hi Marek,

    Can you send me a picture of your schematic? Do you have any passives on PJ.0?

    Thanks,

    Mitch

  • Hi Mitch.

    I have PJ.0 connected to an SPI LORA module (RF95), SPI clock input, thought a 22Ω resistor in series. No other passives present, However, I get the same behaviour with the pin floating and not connected to anything  - 2 out of the 3 devices I tested did not have the LORA module or the 22Ω resistor populated and the pin behaved in the same way. Electrically the pin is fine for sure (no shorts to other signals and good connection of its own), as it works just fine when configured as a GPIO.

    I've attached the relevant part of the board, with PJ.0 hi-lighted. 

  • Hi Marek,

    I ran some tests on my end on an FR6043 EVM, and I saw the same thing as you - MOSI data was being output, but no clock signal was visible. 

    When I explicitly set PJ.0 as an output, I got the SPI clock signal to show up. 

    Try adding:

    PJDIR |= BIT0;

    after line 29 in your SW.

    I think this has something to do with the fact that that pin is muxed with JTAG functionality.

    Please let me know if this resolves the issue.

    Thanks!

    -Mitch

**Attention** This is a public forum