This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/MSP432-RTOS: Using LwIP on MSP432

Part Number: MSP432-RTOS


Tool/software: TI-RTOS

Hello!

I have NFC bank card reader, it uses RS232 and PPP to connect to bank host. Also i have SIM800 for internet connection.

I want to use MSP432 between NFC-reader and SIM800 as a UART-TCP/IP converter. To do this, i need library like LwIP. Can i install it to MSP432?

May be you can point me to the relative examples?

Any ideas about UART-TCP/IP converter?

**Attention** This is a public forum