This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430FR6989: MSP low-power microcontroller forum

Part Number: MSP430FR6989
Other Parts Discussed in Thread: MSP430WARE, MSP-EXP430F5529LP, MSP-EXP430FR5969

Tool/software: Code Composer Studio

Im trying to work through the MSP430 workshop, its been really good so far, until now

Ive gotten to lab10a im asked to import "Command-line interface with LED On.Off/  Flash from the HID examples in MSP430ware, however this doesnt exist for me.

I tried using the H1_LedOnOff example, but its for a different controller and i couldn't get it to function. For some reason no solution files are provided with these labs.

If someone could help me get this lab working i would be very grateful 

   

  • Hello Timothy,

    Welcome to the E2E forums.  I'm glad you've found the MSP Workshop material useful!  It seems like you've been working through most the examples, so could you give me some more feedback.  I'd like to provide any feedback for future updates to the training material.    

    • Have you worked through all the other labs already? 
    • How did they go, any other roadbumps? 
    • Any topics, sections, or labs you think could be improved?   

    As for lab 10, this is obviously an USB lab.  The only MSP430's that have built-in USB are the MSP430F5xx and MSP430F6xx devices.  The only launchpad that this lab will work with is the MSP-EXP430F5529LP which is the device that the example you found is for.  

    This means that you can not work through this USB lab section with your current MSP-EXP430FR5969, as the MSP just does not have an USB module. 

    Thanks,

    JD

**Attention** This is a public forum