Part Number: MSP430F5437A
Other Parts Discussed in Thread: ADS7924
Greetings,
We recently discovered a design error on a product that was manufactured in fairly low quantity (500-700 units) spread over a period of 8 years. The symptoms of that design error did not present themselves until recently in the production run. Our mistake was connecting together DVCC, AVCC, and VCore together at +1.8V. The symptoms were unreliable startup/POR/BOR.
The datasheet is very clear about VCore and our mistake is obvious: "VCORE is for internal use only. No external current loading is possible. VCORE should be connected to only the recommended capacitor value, CVCORE."
The products we delivered with this design mistake went through production testing consisting of temperature cycling and repeated power cycling for each unit. They were operating correctly and reliably until our recent production batch, and some delivered units have had many thousands of hours of operation.
My question is, does TI believe there to be a risk of IC failure due to this design mistake? Is there a reasonable risk that the silicon of the MSP430 could become damaged from shorting VCore to the DVCC/AVCC pins and allowing operation?
Thank you!