Part Number: MSP430F6726A
Hi,
If the fsd24 clock frequency is 8 MHz, what is the effective resolution when the OSR is 1 to 1024?
best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F6726A
Hi,
If the fsd24 clock frequency is 8 MHz, what is the effective resolution when the OSR is 1 to 1024?
best regards,
Hello,
Figure 5-19 in the datasheet illustrates how the SINAD increases as the OSR increases. For a given OSR (e.g. 256), you can convert the SINAD to ENOB using the equation in the following thread.
MSP430I2040 4 channel differential ADC for high resolution measurement
Regards,
James
Hi
Thank you for answering.
By the way, can ENOB and effective resolution be the same calculation method?
Best Regards,
ENOB stands for "effective number of bits", so they could mean the same thing depending on your definition of "effective resolution". ENOB indicates the number of noise-free bits measured for a certain ADC configuration. Hope that helps!
Regards,
James
**Attention** This is a public forum