1.hardware: BOOSTXL-DRV8323Rx BoosterPack™ + MSP430F5529 XL LaunchPad development kit
2.Software: DRV8323_MSP430F5529_Trapezoidal_Sensored_BLDC
3. According to the above software and hardware, the motor can run normally, but when I put a load on the motor,
the motor speed decreases and cannot return to the set speed.I need to keep the speed constant while loading the motor,
How can I solve this problem?
4.If the above problems can not be solved, please recommend a trapezoidal_Sensored_BLDC scheme?
The solution consists of software and hardware.
(Voltage 30V, current 15A,Hall,trapezoidal_Sensored_BLDC)