Part Number: MSP432P401R
Hi,
I have found this:
Acording to that, the input resistance is very low.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My mistake, I wrote my question too quikly.
Hello,
The table you show with the 2Kohms is for the comparator and not the ADC. Please refer to 5.26.7, Table 5-27 and the parameter Ri which can typically be about 135 ohms. Also refer to Table 5-28 and the parameter tsample. Using the equation found in note 4 you can determine is the sample and hold time is adequate for the impedance in your setup. This includes the impedance of the ADC as well as the source impedance of what is being measured. If an acceptable sample time cannot be achieved with the impedances of the system, then it is recommended to add a simple voltage follower to reduce the source impedance.
Regards,
Chris
We will do the maths and add a voltage follower to see what works better.
Thank you very much.
**Attention** This is a public forum