I used a MSP430FR6877 IPNR, an application code in a year after the operation of the phenomenon of continuous reset, re-power can not be resolved, I tried to check the hardware power supply, reset circuit, crystal oscillator, no problem, and did A to B cross-test, I wrote a minimum system code, configure only P7. 6IO, when I set the output of P7.6 to reproduce the problem that can be 0, and set the output of p7.6 to 1, the problem was solved.