Part Number: TSS721A
Hello!
We have a problem with output VDD of TS721A. We got voltage on the VDD pin 2.2V. Why?
RRIDD=30k, RRIS=100, CSTC=47uF, CSC=220nF
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TSS721A
Hello!
We have a problem with output VDD of TS721A. We got voltage on the VDD pin 2.2V. Why?
RRIDD=30k, RRIS=100, CSTC=47uF, CSC=220nF
Hello Egor,
Do you have a load on the VDD pin when you see 2.2V? If so, it could be that your load is pulling too much current dragging the voltage down. You could try a larger capacitor on Cstc.
We don't have a load on the VDD pin. Voltage on the STC pin 3.9 V, so VDD is off. How to increase the voltage VSTC?
Egor,
Is your bus voltage within the minimum and maximum ranges shown on page 8 of the datasheet? If so, have you also tried using the values shown in figure 7 of the datasheet?
**Attention** This is a public forum