This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi,
I currently have a program that uses the onboard buttons as interrupts to toggle the LEDs, but for some reason, the interrupt function is called before the buttons are ever pressed.
I used the command P5IFG &= ~(BIT5 + BIT6); to clear the interrupt flags before the IO pins were unlocked, so I am unsure of why this is happening. Can someone please explain why this is happening?
My program is shown here:
#include <msp430.h> volatile int flag1 = 0; volatile int flag2 = 0; /** * main.c */ int main(void) { WDTCTL = WDTPW | WDTHOLD; // stop watchdog timer //Configure Unused Pins to the lowest power State (Output direction, tied low) P1OUT = 0; P1DIR = 0xFF; P2OUT = 0; P2DIR = 0xFF; P3OUT = 0; P3DIR = 0xFF; P4OUT = 0; P4DIR = 0xFF; P5OUT = 0; P5DIR = 0xFF; P6OUT = 0; P6DIR = 0xFF; P7OUT = 0; P7DIR = 0xFF; P8OUT = 0; P8DIR = 0xFF; PJOUT = 0; PJDIR = 0xFF; //Enable internal pull-up/down resistors P5REN |= BIT5 + BIT6; //Required to set pull-up high resistor P5OUT |= BIT5 + BIT6; //Set P5.5 and P5.6 as input pins P5DIR &= (~BIT5); P5DIR &= (~BIT6); //Falling Edge P5IES = BIT5 + BIT6; //Clear interrupt flags P5IFG &= ~(BIT5 + BIT6); //Enable interrupts P5IE = BIT5 + BIT6; PM5CTL0 &= ~LOCKLPM5; // Disable the GPIO power-on default high-impedance mode // to activate previously configured port settings __enable_interrupt(); while(1){ if (flag1 == 1){ P1OUT ^= BIT0; flag1 = 0; } if (flag2 == 1){ P1OUT ^= BIT1; flag2 = 0; } } } //Port 5 interrupt service routine #pragma vector=PORT5_VECTOR __interrupt void Port_1(void){ flag1 = 1; flag2 = 1; P5IFG &= ~(BIT5 + BIT6); }
Thanks,
John
Bruce,
Thank you, I missed that in the User Guide. It seems that by clearing LOCKLPM5, the interrupt flags that were controlling the button interrupt were set.
My program works as intended now.
Thanks,
John
Hi John,
Thanks for using MSP430 devices. Please feel free to come back to E2E if you have any technical issue or question.
**Attention** This is a public forum