This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-GANG430: Using script as standalone feature?

Part Number: MSP-GANG430

I have a project which uses 2 MSP430 microcontrollers. I would like to program both of them in the same 'jig' using the same MSP-GANG programmer. To do this, I have written a script that will program one MSP, then the other. This works fine when I have the GANG software and I run from Script file. However, I want to use the programmer as a Standalone unit in production. Is there a way to do this? I cannot seem to save the script to an image, nor will it work on an SD card. 

I am fine with using the GANG program, but we are not too keen on production staff accessing it and potentially making unwanted changes, hence wanting the script to work on the standalone unit.

I have tried finding an answer on Google but have yet to find anything. Is this possible or am I just going to have to give up and use 2 programmers to do the programming on this one project? It seems a waste as I will only be using 1 port on each programmer so if there is a way to just run the script, that would be great.

**Attention** This is a public forum