This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
i am using MSP432EA01Y LAUNCHPAD with cc2650moda (BLE). When i connect MSP432EA01Y LAUNCHPAD using usb cable with my laptop i should get 3.3V or 5V from the pins which indicate voltage. When I measure voltage at that pins using multimeter i am not getting 3.3V or 5V .
Whats the issue or how to supply MSP432EA01Y LAUNCHPAD to get 3.3 V
Thanks
My Launchpad shows 3.3V on the J1+J5+J12 3V3 pins and 5V (really 4.8V) on the J3+J7+J13 5V pins.
Do you have the jumpers installed on J101 ("bridge header")? Is your USB connected to the XDS110 end of the board?
I don't have a CC2650MODA Booster Pack. Try removing it.
**Attention** This is a public forum